2013-09-13 5:04 PM
Hello,
I tried to read two analog inputs from PA3(ADC1_IN3) and PA5(ADC1_IN5). I expected tmpADC[0] has the input data of PA3 and tmpADC[1] has the input data of PA5. However, both tmpADC[0] and tmpADC[1] always have the input data of PA3. I read reference manual multiple times, but I couldn't figure out what is wrong. Please let me know what is problem. I attached my code below(only ADC part). Thanks &sharpinclude <stm32f4xx.h> void ADC_Init(void) { GPIOA->MODER |= (3UL<<6)|(3UL<<10); /*Set PA3 as an analog input, ADC1_IN3, Set PA5 as an analog input ADC1_IN5*/ GPIOA->PUPDR &= ~((3UL<<6)|(3UL<<10)); /*No Pull up and down resistor*/ RCC->APB2ENR =(1<<8); /*ADC1 clk enable*/ ADC1->CR1 = 0; ADC1->CR2 = (1UL<<0)| /*ADC1 power on */ (1UL<<1); /*Continuous conversion*/ ADC1->SMPR1 = 0; ADC1->SMPR2 = 0; ADC1->SQR1 = (1<<20); /* sequence length: two regular conversions*/ ADC1->SQR2 = 0; ADC1->SQR3 = (3UL<<0)|(5UL<<5); /*1st conversion = ADC1_lN3, 2nd conversion = ADC1_IN5*/ ADC->CCR = (1UL<<16); /*fpclk2/4 = 21Mhz */ } short unsigned int get_ADC(void) { ADC1->CR2 |= (1<<30); while(!(ADC1->SR & 0x2)); return ADC1->DR; } int main (void) { tmpADC[0] = get_ADC(); // expecting have data from ADC1_IN3 tmpADC[1] = get_ADC(); //expecting have data from ADC1_IN5 } #stm32f4 #discovery-board #adc-dma2013-10-08 1:35 PM
I've built a 5x version in Keil that seems serviceable, and produces values in the 0-4095 range, not sure what's going on here.
2013-10-08 10:41 PM
Well I tried the code in a new project and it worked flawlessly even though the code running was identical. Very strange. Thank you for your help.
Chris2014-04-17 2:20 PM
What's the cut-off for ''slow speed''?
2014-04-17 2:32 PM
What's the cut-off for ''slow speed''?
SampleTime+12 vs your ability to service the EOC interrupt. I haven't plotted the curve, DMA requires no thought.The total conversion time is calculated as follows:
Tconv = Sampling time + 12 cycles
Example:
With ADCCLK = 30 MHz and sampling time = 3 cycles:
Tconv = 3 + 12 = 15 cycles = 0.5 μs with APB2 at 60 MHz
2015-01-12 8:46 AM
Clive1
I used your first posted program with a little modification to convert the same channel for 8 times, but I find only the first 4 conversions are ''correct'' and the second 4 conversions are ''wrong''. What is wrong in the program? Please help. the converted values are: 0x819, 0x817, 0x818, 0x818, 0x6F8, 0x638, 0x517, 0x464 The values get smaller and smaller.typedef struct {
int chn_nr; //total channels
uint8 chn[TOTAL_CHN];
} ADCDev;
//const ADCDev adc1 = {8, { 4, 4, 4, 4, 4, 4, 4, 4 } };
const ADCDev adc1 = {8, {16, 16, 16, 16, 16, 16, 16, 16} };
void ADC_Configuration(uint16_t *ADCConvertedValues)
{
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
/* Enable peripheral clocks *************************************************/
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
/* DMA2_Stream0 channel0 configuration **************************************/
DMA_DeInit(DMA2_Stream0);
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)ADCConvertedValues;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = ADC1;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; ///
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
/* DMA2_Stream0 enable */
DMA_Cmd(DMA2_Stream0, ENABLE);
/* ADC Common Init **********************************************************/
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
ADC_TempSensorVrefintCmd(ENABLE);
/* ADC1 Init ****************************************************************/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = adc1.chn_nr;
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channel configuration ******************************/
//ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 1, ADC_SampleTime_480Cycles); // PA3
//ADC_RegularChannelConfig(ADC1, ADC_Channel_5, 2, ADC_SampleTime_480Cycles); // PA5
for (int i=0;i<sizeof(adc1.chn_nr);i++)
ADC_RegularChannelConfig(ADC1, adc1.chn[i], i+1, ADC_SampleTime_3Cycles);
/* Enable DMA request after last transfer (Single-ADC mode) */
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 **************************************************************/
ADC_Cmd(ADC1, ENABLE);
/* Start ADC1 Software Conversion */
ADC_SoftwareStartConv(ADC1);
}
2015-01-12 10:09 AM
DMA_InitStructure.DMA_BufferSize = ADC1;
//????
2015-01-12 12:07 PM
2015-01-12 12:17 PM
The question is still the same, why one the first 4 conversions are OK? I even tried to convert 16 times, but it is only the first 4 are reasonable, and the values are getting smaller and smaller after 4 conversion.
I guess you'd have to ponder the ability of the signal source to supply current to charge the capacitor in the sample circuit, and the sample time?