cancel
Showing results for 
Search instead for 
Did you mean: 

Multi Channel ADC on 1 DMA

blue_dolphin1987
Associate II
Posted on December 17, 2013 at 11:11

Hi i am trying to scan 4 channel using ADC1 and DMA1.

At the end of 1 cycle i will restart the acquision process (triggered in DMA TC interrupt handler). However i realised that it seem on every run the result of my conversion is different when noting is changed e.g. 1st run 2nd Run 3rd Run 0x00000FFF

0x00000

FFF

0x00000000

0x00000000

0x00000

FFF

0x00000000

0x00000000

0x00000000 0x00000000

0x00000000

0x00000000 0x00000

FFF

void NVIC_Configuration(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable the USART1 TX DMA Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
void DMA_Configuration(void){
/* DMA1 channel1 configuration ----------------------------------------------*/
DMA_DeInit(DMA1_Channel1);
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)ADC_DualConvertedValueTab;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_BufferSize = 16;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA1_Channel1, &DMA_InitStructure);
/* Enable DMA Stream Transfer Complete interrupt */
DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE);
/* Enable DMA1 Channel1 */
DMA_Cmd(DMA1_Channel1, ENABLE);
}
void ADC_Configuration(void){
/* ADC1 configuration ------------------------------------------------------*/
ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; 
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel = 4;
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channels configuration */ 
ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 1, ADC_SampleTime_239Cycles5); 
ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 2, ADC_SampleTime_239Cycles5);
ADC_RegularChannelConfig(ADC1, ADC_Channel_13, 3, ADC_SampleTime_239Cycles5); 
ADC_RegularChannelConfig(ADC1, ADC_Channel_14, 4, ADC_SampleTime_239Cycles5); 
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
}
void ADC_Calibration(void){
/* Enable ADC1 reset calibration register */ 
ADC_ResetCalibration(ADC1);
/* Check the end of ADC1 reset calibration register */
while(ADC_GetResetCalibrationStatus(ADC1));
/* Start ADC1 calibration */
ADC_StartCalibration(ADC1);
/* Check the end of ADC1 calibration */
while(ADC_GetCalibrationStatus(ADC1));
}
void Start_Conversion(void){
/* Start ADC1 Software Conversion */ 
ADC_SoftwareStartConvCmd(ADC1, ENABLE);
}
void DMA1_Channel1_IRQHandler(void){
/* Test on DMA Transfer Complete interrupt */
if (DMA_GetITStatus(DMA1_IT_TC1)) 
{ 
ADC_DMA_Configuration();
ADC_Start_Conversion();
/* Clear DMA Transfer Complete interrupt pending bit */
DMA_ClearITPendingBit(DMA1_IT_TC1);
/* ... */
}
}

Did i miss something ? Thanks. #adc-and-dma #wait-for-you--clive1-!-!-!
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on December 17, 2013 at 13:11

Did i miss something ?

There appears to be a lot of code/definitions missing, making it undesirable to dig into it. Observe how I present my examples.

Why 16x 32-bit words for the DMA transfer?

Why continuous mode, if you just want four samples?

I think this would be more robust if you just set this up once, in circular mode, and using HT/TC interrupts

Clear the TC before doing the re-initialization.

Do not enable DMA prior to doing calibration
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
blue_dolphin1987
Associate II
Posted on December 18, 2013 at 03:00

void RCC_Configuration(void)
{
/* ADCCLK = PCLK2/4 */
RCC_ADCCLKConfig(RCC_PCLK2_Div2);
/* Enable peripheral clocks ------------------------------------------------*/
/* Enable DMA1 clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
/* Enable ADC1, ADC2 and GPIOC clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_ADC2 |
RCC_APB2Periph_GPIOC, ENABLE);
}
/**
* @brief Configures the different GPIO ports.
* @param None
* @retval None
*/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure; 
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
void NVIC_Configuration(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable the USART1 TX DMA Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
void DMA_Configuration(void){
/* DMA1 channel1 configuration ----------------------------------------------*/
DMA_DeInit(DMA1_Channel1);
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)ADC_DualConvertedValueTab;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_BufferSize = 16;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA1_Channel1, &DMA_InitStructure);
/* Enable DMA Stream Transfer Complete interrupt */
DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE);
/* Enable DMA1 Channel1 */
DMA_Cmd(DMA1_Channel1, ENABLE);
}
void ADC_Configuration(void){
/* ADC1 configuration ------------------------------------------------------*/
ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; 
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel = 4;
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channels configuration */ 
ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 1, ADC_SampleTime_239Cycles5); 
ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 2, ADC_SampleTime_239Cycles5);
ADC_RegularChannelConfig(ADC1, ADC_Channel_13, 3, ADC_SampleTime_239Cycles5); 
ADC_RegularChannelConfig(ADC1, ADC_Channel_14, 4, ADC_SampleTime_239Cycles5); 
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
}
void Calibration(void){
/* Enable ADC1 reset calibration register */ 
ADC_ResetCalibration(ADC1);
/* Check the end of ADC1 reset calibration register */
while(ADC_GetResetCalibrationStatus(ADC1));
/* Start ADC1 calibration */
ADC_StartCalibration(ADC1);
/* Check the end of ADC1 calibration */
while(ADC_GetCalibrationStatus(ADC1));
}
void Start_Conversion(void){
/* Start ADC1 Software Conversion */ 
ADC_SoftwareStartConvCmd(ADC1, ENABLE);
}
void DMA1_Channel1_IRQHandler(void){
/* Test on DMA Transfer Complete interrupt */
if (DMA_GetITStatus(DMA1_IT_TC1)) 
{ 
/* Clear DMA Transfer Complete interrupt pending bit */
DMA_ClearITPendingBit(DMA1_IT_TC1); 
ADC_DMA_Configuration();
ADC_Start_Conversion();
}
}
int main(void) {
RCC_Configuration();
NVIC_Configuration();
GPIO_Configuration();
ADC_Configuration();
Calibration();
DMA_Configuration();
Start_Conversion();
}
__IO uint32_t ADC_DualConvertedValueTab[16];

Hi Clive i made some changes and added the full code however the issues persist. Thanks. In addition , may i know what is the different between the following 2

uint32_t DMA_PeripheralDataSize; 
/*!< Specifies the Peripheral data width.
This parameter can be a value of @ref DMA_peripheral_data_size */
uint32_t DMA_MemoryDataSize; 
/*!< Specifies the Memory data width.
This parameter can be a value of @ref DMA_memory_data_size */

Posted on December 18, 2013 at 16:12

Still seems to be missing routines, and some indication of processor/board being used. The goal is to present some code I can drop in a compiler, and evaluate.

Suggest you tie one of the pins to a reference (1.8V or 1.2V perhaps) so you can confirm it's position in the array, if your problem is one of it randomly starting at the wrong channel, or slipping.

In circular mode you don't reinitialize the DMA, and start the ADC, it keeps going. The need for 16 samples in a continuous fashion wasn't really addressed.

Here's an example of 3 channels on a STM32 VL-Discovery board, observe how it is presented.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/DMA1_Channel1_IRQHandler&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=119]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FDMA1_Channel1_IRQHandler&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=119

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
blue_dolphin1987
Associate II
Posted on December 19, 2013 at 03:48

Hi Clive1 , i am using STm32f1 . 

It seems to be the case which the conversion result is slipping. 

The reason  for 16 samples is to collect 4 sample from each of the 4 channel for averaging purpose. I only require the conversion at fixed interval of 500. 

So my idea is to on the ADC and DMA to collect 16 samples and then off it . When a timer of 500ms  lapse i will enable ADC and DMA to collect 16 samples again.