Question
Multi channel ADC conversion with DMA and Interrupt.
hello everyone,
i am new to STM32 controller series,
i am trying to read mutli channel ADC with help of DMA and Interrupt.but facing issue.
i am not getting ok status from"HAL_ADC_Start_DMA" this function.
can any-body help me out.
please find below configuration code.
kindly guide me, where i am wrong.
static void ADCx_Init(void)
{
/* Set ADC instance */
hnucleo_Adc.Instance = NUCLEO_ADCx;
if (HAL_ADC_GetState(&hnucleo_Adc) == HAL_ADC_STATE_RESET)
{
/* ADC Config */
hnucleo_Adc.Instance = ADC1;
hnucleo_Adc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV256;
hnucleo_Adc.Init.Resolution = ADC_RESOLUTION_12B;
hnucleo_Adc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hnucleo_Adc.Init.ScanConvMode = ADC_SCAN_ENABLE;
hnucleo_Adc.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hnucleo_Adc.Init.LowPowerAutoWait = DISABLE;
hnucleo_Adc.Init.ContinuousConvMode = ENABLE;
hnucleo_Adc.Init.NbrOfConversion = 2;
hnucleo_Adc.Init.DiscontinuousConvMode = DISABLE;
hnucleo_Adc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hnucleo_Adc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hnucleo_Adc.Init.DMAContinuousRequests = ENABLE;
hnucleo_Adc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hnucleo_Adc.Init.OversamplingMode = DISABLE;
/* Initialize ADC */
HAL_ADC_Init(&hnucleo_Adc);
/**Configure Regular Channel */
sConfig.Channel = ADC_CHANNEL_15;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hnucleo_Adc, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure Regular Channel */
sConfig.Channel = ADC_CHANNEL_16;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hnucleo_Adc, &sConfig) != HAL_OK)
{
while(1);
}
if (HAL_ADC_Start_DMA(&hnucleo_Adc,
(uint32_t *)aADCxConvertedData,
ADC_CONVERTED_DATA_BUFFER_SIZE
) != HAL_OK)
{
while(1);
}
}
}void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{
GPIO_InitTypeDef GPIO_InitStruct;
if(hadc->Instance==ADC1)
{
/* USER CODE BEGIN ADC1_MspInit 0 */
/* USER CODE END ADC1_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_ADC_CLK_ENABLE();
/**ADC1 GPIO Configuration
PB0 ------> ADC1_IN15
PB1 ------> ADC1_IN16
*/
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG_ADC_CONTROL;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* ADC1 DMA Init */
/* ADC1 Init */
hdma_adc1.Instance = DMA1_Channel2;
hdma_adc1.Init.Request = DMA_REQUEST_ADC1;
hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_adc1.Init.Mode = DMA_CIRCULAR;
hdma_adc1.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);
/* ADC1 interrupt Init */
HAL_NVIC_SetPriority(ADC1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(ADC1_IRQn);
/* USER CODE BEGIN ADC1_MspInit 1 */
/* USER CODE END ADC1_MspInit 1 */
}
}void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMAMUX1_CLK_ENABLE();
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Channel2_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel2_IRQn);
}Thanks!!!