cancel
Showing results for 
Search instead for 
Did you mean: 

Mistake?

franck2
Associate II
Posted on December 10, 2014 at 11:10

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
franck2
Associate II
Posted on December 10, 2014 at 11:19

I found an error in the code:

clock of TIM15 and TIM16 not enabeled.

Actually:

  /* TIM2, TIM3 and TIM4 clock enable */

 

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM3 | RCC_APB1Periph_TIM4 , ENABLE);

Should be replaced by:

  /* TIM2, TIM15 and TIM16 clock enable */

 

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

 

   RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM16, ENABLE);

 

   RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM15, ENABLE);

Amel NASRI
ST Employee
Posted on December 10, 2014 at 15:18

No TIM3 or TIM4 available for that STM32F302!

That is true only for STM32F302x6/8. These 2 timers are available in STM32F302xB/C.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

franck2
Associate II
Posted on December 17, 2014 at 17:33

I'm trying to port the ST TIM_Synchronization to my evaluation board Nucleo STM32F302R8T6 without success.

I used only 2 cascaded timers TIM1 & TIM2.

TIM1 is configured as Master Timer:

         - PWM Mode is used

         - The TIM1 Update event is used as Trigger Output  

TIM2 is slave for TIM1

         - PWM Mode is used

         - The ITR1(TIM1) is used as input trigger

         - Gated mode is used, so start and stop of slave counter are controlled by the Master trigger output signal(TIM1 update event).

Here is my code:

/**

 

  ******************************************************************************

 

  * @file    TIM/TIM_Synchronization/main.c  

 

  ******************************************************************************

 

  */

 

 

/* Includes ------------------------------------------------------------------*/

 

#include ''stm32f30x.h''

 

 

/* Private function prototypes -----------------------------------------------*/

 

static void TIM_Config(void);

 

/* Private functions ---------------------------------------------------------*/

 

 

 

/**

 

  * @brief  Configure the TIMs.

 

  * @param  None

 

  * @retval None

 

  */

 

static void TIM_Config(void)

 

{

 

  GPIO_InitTypeDef GPIO_InitStructure;

 

  TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

 

  TIM_OCInitTypeDef  TIM_OCInitStructure;

 

    int Prescaler, Period;

 

    

 

    /* TIM2, TIM1 clock enable */

 

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);

 

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

 

    

 

    /* GPIOA clocks enable */

 

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

 

    

 

  /* GPIOA Configuration: TIM2_CH1 as alternate function push-pull */

 

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

 

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

 

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

 

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;

 

    

 

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 ;

 

  GPIO_Init(GPIOA, &GPIO_InitStructure);

 

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_6); // TIM1_CH1 PA8 AF6    

 

 

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 ;

 

  GPIO_Init(GPIOA, &GPIO_InitStructure);

 

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_1); // TIM2_CH1 PA0 AF1

 

 

  Prescaler = (SystemCoreClock / 8000000); // 8 MHz timebase, assumes APB2 H/1 TIMCLK1 H/1

 

  Period = 8000000 / 200000; // 8 MHz -> 200 KHz

 

            

 

  /* Time base configuration */

 

  TIM_TimeBaseStructure.TIM_Period = Period - 1;

 

  TIM_TimeBaseStructure.TIM_Prescaler = Prescaler - 1;

 

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

 

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

 

  TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);

 

 

 

  /* Master Configuration in PWM1 Mode */

 

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

 

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

 

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

 

  TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset;

 

 

 

  TIM_OCInitStructure.TIM_Pulse = Period / 2; // 50%

 

  TIM_OC1Init(TIM1, &TIM_OCInitStructure);

 

 

 

    /* Enable pins, TIM1 more sensitive */    

 

    TIM_CtrlPWMOutputs(TIM1, ENABLE);

 

    

 

  /* TIM1 enable counter */    

 

    TIM_Cmd(TIM1, ENABLE);

 

 

  /* Timers synchronisation in cascade mode ----------------------------

 

     1/TIM1 is configured as Master Timer:

 

         - PWM Mode is used

 

         - The TIM1 Update event is used as Trigger Output  

 

 

     2/TIM2 is slave for TIM1

 

         - PWM Mode is used

 

         - The ITR1(TIM1) is used as input trigger

 

         - Gated mode is used, so start and stop of slave counter

 

           are controlled by the Master trigger output signal(TIM1 update event).

 

  --------------------------------------------------------------------------- */

 

    

 

  /* Select the Master Slave Mode */

 

  TIM_SelectMasterSlaveMode(TIM1, TIM_MasterSlaveMode_Enable);

 

 

  /* Master Mode selection */

 

  TIM_SelectOutputTrigger(TIM1, TIM_TRGOSource_Update);

 

 

  /* Slaves Configuration: PWM1 Mode */

 

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

 

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;    

 

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;    

 

 

  TIM_OCInitStructure.TIM_Pulse = Period / 2;

 

 

  TIM_OC1Init(TIM2, &TIM_OCInitStructure);

 

 

  /* Slave Mode selection: TIM2 */

 

  TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Gated);

 

  TIM_SelectInputTrigger(TIM2, TIM_TS_ITR1);

 

 

  /* TIM enable counter */

 

  TIM_Cmd(TIM2, ENABLE);

 

 

}

 

 

/**

 

  * @brief  Main program.

 

  * @param  None

 

  * @retval None

 

  */

 

int main(void)

 

{

 

  /*!< At this stage the microcontroller clock setting is already configured,

 

       this is done through SystemInit() function which is called from startup

 

       file (startup_stm32f30x.s) before to branch to application main.

 

       To reconfigure the default setting of SystemInit() function, refer to

 

       system_stm32f30x.c file

 

     */

 

 

  /* TIMs Configuration */

 

  TIM_Config();

 

 

  /* Infinite loop */

 

  while (1)

 

  {

 

  }

 

}

 

#ifdef  USE_FULL_ASSERT

 

 

/**

 

  * @brief  Reports the name of the source file and the source line number

 

  *         where the assert_param error has occurred.

 

  * @param  file: pointer to the source file name

 

  * @param  line: assert_param error line source number

 

  * @retval None

 

  */

 

void assert_failed(uint8_t* file, uint32_t line)

 

{

 

  /* User can add his own implementation to report the file name and line number,

 

     ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

 

 

  /* Infinite loop */

 

  while (1)

 

  {

 

  }

 

}

 

#endif

 

 

/**

 

  * @}

 

  */

 

 

/**

 

  * @}

 

  */

 

 

/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

Thanks for any help.

franck2
Associate II
Posted on December 18, 2014 at 10:54

Any avalaible help?

Or working example?

Thanks

franck2
Associate II
Posted on December 18, 2014 at 11:19

Is there some internal trigger connection?

Changing from ITR0 gives result.