2018-06-29 1:33 AM
I'm working at ARM Germany and using Keil MDK with the STM32L1xx_DFP pack v1.2.0
According to the definition from
the following bits of RCC_CSR register (page 165) for STM32L152xx are missing in System Viewer file STM32L15x.svd:
bit 11 LSECSSONbit 12 LSECSSDbit 25 OBLRSTFand for RCC_CIR (page 144):
bit 14 LSECSSIEbit 22 LSECSSCI can reproduce this issue with STM32L152RE Nucleo board.
2018-06-29 1:49 AM
Hello Chen,
I have reported your point internally for check. We will keep you posted about any further update.
Khouloud.