cancel
Showing results for 
Search instead for 
Did you mean: 

Microxplorer suggestions for improvement

asrock70
Associate II
Posted on October 02, 2013 at 10:05

Maybe it

's

read by

developers from ST.

I

had

two

ideas for

improvements

-

Somehow

graphically

distinguish

outputs that

are

5

volt

tolerant

- A

dd

user defined (

label)

tag

in

which

the

user

can

observe

what

signal

is

connected

to the

pin.

It

streamlines the

design and

should

be

added

export

in

jpg

etc

.,

I could use

it

for

project documentation

#microxplorer
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
bernard
Associate
Posted on October 07, 2013 at 15:47

I agree: it would be nice to to redefine the standard pin names with user names, e.g. the signal names used on the schematics. It's easy to then generate a table of correspondance in the program with #define. Thanks to the team for the nice tool, however.

tim239955_stm1
Associate II
Posted on October 17, 2013 at 19:09

I agree. A user defined label field for each pin would be very useful. I mentioned it to an ST rep quite a while back but probably got lost. They could use a feedback link somewhere in the Microxplorer section of the web site as I don't think they monitor these forums very closely.

Posted on October 17, 2013 at 19:17

I don't think they monitor these forums very closely.

Indeed, it's a user forum.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
tim239955_stm1
Associate II
Posted on July 09, 2014 at 23:21

But moderated and therefore should be monitored. STM32CubeMX has incorporated our suggestion of user names for the pins (not sure when but V4.3.0 has it). Nothing to indicate 5V tolerance that I can see yet.