2009-01-21 08:43 AM
MICRO sd CARD INTERFACED THROUGH SPI ?
2011-05-17 04:00 AM
Is it possible to interface micro SD Card through SPI of STM32F103VET6.
I cannot use the SDIO pins as all the serial ports are reqd . and they are multiplexed with it . Also can anyone provide me with a link to the datasheet providing the pin configuration of a MicroSD Card ADAPTOR as it will be reqd. also . Thanks..2011-05-17 04:00 AM
You really should start with google before posting here. Offers me tons and tons of result for ''microsd spi pinout''.
Here's one that should suit your needs: http://www.tayloredge.com/reference/Interface/SDPINOUT.pdf -Relaxe2011-05-17 04:00 AM
Quote:
You really should start with google before posting here. Offers me tons and tons of result for ''microsd spi pinout''.
See: