cancel
Showing results for 
Search instead for 
Did you mean: 

Meaning off GPIO_Speed declaration

infoinfo973
Associate II
Posted on November 04, 2010 at 09:38

Meaning off GPIO_Speed declaration

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
John F.
Senior
Posted on May 17, 2011 at 14:13

Please see RM0008 Reference manual section 8.1.

Output MODE bits

MODE[1:0] Meaning

00 Reserved

01 Max. output speed 10 MHz

10 Max. output speed 2 MHz

11 Max. output speed 50 MHz

Also see the Data Sheet for your device and look at the Electrical characteristics / Input/output AC characteristics. Basically, choose lower speed if you don't need fast clocks or edge transitions. It will reduce EMC problems.

Posted on May 17, 2011 at 14:13

See also SLEW RATE CONTROL

If you drive the pin aggressively to get sharp edges, and over come line capacitance, you will typically see more over-shoot/under-shoot, and ringing, in the output signal.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
dthedens2
Associate II
Posted on May 17, 2011 at 14:13

Well, he does have a point.  Table 19 shows these values for MODE.  But no where does RM0008 explain what they mean.  The STM32F103ZE (which I use) data sheet table 47 has some additional info, but not much.

WHat really happens when MODE is set to 10 and the code performs a pin high and then a pin low?

For that info, one has to go to other ARM vendor documentation and hope that the ST works the same.