cancel
Showing results for 
Search instead for 
Did you mean: 

Compatibility of X-NUCLEO-IKS4A1 with X-NUCLEO-WB05KN1 or BLE Expansion Options for NUCLEO-U575ZI-Q

Duc
Senior

Hello STM Community,

I currently have a NUCLEO-U575ZI-Q board and the X-NUCLEO-IKS4A1 motion MEMS and environmental sensor expansion board. I’m looking to add BLE functionality and was considering the X-NUCLEO-WB05KN1.

Before proceeding, I’d like to ask:

  1. Are the X-NUCLEO-IKS4A1 and X-NUCLEO-WB05KN1 compatible when stacked together on the NUCLEO-U575ZI-Q?

  2. If not, is there an alternative BLE expansion board that is known to work well with the IKS4A1 on this Nucleo board?

  3. Alternatively, is there an expansion or adapter board that allows both shields to be connected without pin conflicts?

Any guidance or shared experience would be greatly appreciated!

Thanks in advance.

0 REPLIES 0