cancel
Showing results for 
Search instead for 
Did you mean: 

Mcsdk installer for linux

Prasad-konnur
Associate

Using part STM32G4. Wanted to check the referance code for pwm.

Is mcsdk linux download available?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Peter BENSCH
ST Employee

Welcome @Prasad-konnur, to the community!

UM3027 states that X-CUBE_MCSDK currently requires a PC with Windows.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter,

Thanks for the reply.

Can you point me to the referance code for the timer configuration in PWM mode. Any example is available?

If it is only about the timer configuration, you will find plenty of information in AN4013, AN4776 or the reference manual of the respective STM32, i.e. RM0440 for the STM32G4. But you can also create them with STM32CubeMX, which is also available for Linux.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.