cancel
Showing results for 
Search instead for 
Did you mean: 

Maximum rating of the RST terminal of the STM32F765

Knish.1
Associate

In the general operating section, it is described as "Input voltage on RST and FT pins".

Do you consider the maximum rating of the RST pin to be the same as the FT pin?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Uwe Bonnes
Chief

Look in table 18 VIN:

Input voltage on RST and FT pins(8) 

2 V < VDD < 3.6 V - 0.3 - 5.5

     VDD < 2 V      - 0.3 - 5.2