MAX31856 connection problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-11-26 4:50 AM
Hello,
Have a Chinese version CJMCU-31856 with MAX31856 chip on board. Trying to establish connection, data transmit and read temperature from this chip with STM32F407VE using SPI2 port.
But no successful yet. I cannot read any data or transfer any data. Plus unhappily my logic analyzer stops work and I cannot figure out what is going with SPI2 port.
Here is the C and HEX.
Who has a experience working with it? Am I forgot something?
#include "stm32f4xx_hal.h"
#ifndef MAX31856_H
#define MAX31856_H
#define MAX31856_CR0_RREG 0x00 ///< Config 0 read register
#define MAX31856_CR0_WREG 0x80 ///< Config 0 write register
#define MAX31856_CR0_AUTOCONVERT 0x80 ///< Config 0 Auto convert flag
#define MAX31856_CR0_1SHOT 0x40 ///< Config 0 one shot convert flag
#define MAX31856_CR0_OCFAULT1 0x20 ///< Config 0 open circuit fault 1 flag
#define MAX31856_CR0_OCFAULT0 0x10 ///< Config 0 open circuit fault 0 flag
#define MAX31856_CR0_CJ 0x08 ///< Config 0 cold junction disable flag
#define MAX31856_CR0_FAULT 0x04 ///< Config 0 fault mode flag
#define MAX31856_CR0_FAULTCLR 0x02 ///< Config 0 fault clear flag
#define MAX31856_CR1_RREG 0x01 ///< Config 1 read register
#define MAX31856_CR1_WREG 0x81 ///< Config 1 write register
#define MAX31856_MASK_REG 0x02 ///< Fault Mask register
#define MAX31856_CJHF_REG 0x03 ///< Cold junction High temp fault register
#define MAX31856_CJLF_REG 0x04 ///< Cold junction Low temp fault register
#define MAX31856_LTHFTH_REG 0x05 ///< Linearized Temperature High Fault Threshold Register, MSB
#define MAX31856_LTHFTL_REG 0x06 ///< Linearized Temperature High Fault Threshold Register, LSB
#define MAX31856_LTLFTH_REG 0x07 ///< Linearized Temperature Low Fault Threshold Register, MSB
#define MAX31856_LTLFTL_REG 0x08 ///< Linearized Temperature Low Fault Threshold Register, LSB
#define MAX31856_CJTO_REG 0x09 ///< Cold-Junction Temperature Offset Register
#define MAX31856_CJTH_REG 0x0A ///< Cold-Junction Temperature Register, MSB
#define MAX31856_CJTL_REG 0x0B ///< Cold-Junction Temperature Register, LSB
#define MAX31856_LTCBH_REG 0x0C ///< Linearized TC Temperature, Byte 2
#define MAX31856_LTCBM_REG 0x0D ///< Linearized TC Temperature, Byte 1
#define MAX31856_LTCBL_REG 0x0E ///< Linearized TC Temperature, Byte 0
#define MAX31856_SR_REG 0x0F ///< Fault Status Register
#define ON 1
#define OFF 0
#define MAX31856_FAULT_CJRANGE 0x80 ///< Fault status Cold Junction Out-of-Range flag
#define MAX31856_FAULT_TCRANGE 0x40 ///< Fault status Thermocouple Out-of-Range flag
#define MAX31856_FAULT_CJHIGH 0x20 ///< Fault status Cold-Junction High Fault flag
#define MAX31856_FAULT_CJLOW 0x10 ///< Fault status Cold-Junction Low Fault flag
#define MAX31856_FAULT_TCHIGH 0x08 ///< Fault status Thermocouple Temperature High Fault flag
#define MAX31856_FAULT_TCLOW 0x04 ///< Fault status Thermocouple Temperature Low Fault flag
#define MAX31856_FAULT_OVUV 0x02 ///< Fault status Overvoltage or Undervoltage Input Fault flag
#define MAX31856_FAULT_OPEN 0x01 ///< Fault status Thermocouple Open-Circuit Fault flag
/** Noise filtering options enum. Use with setNoiseFilter() */
typedef enum {
MAX31856_NOISE_FILTER_50HZ,
MAX31856_NOISE_FILTER_60HZ
} max31856_noise_filter_t;
/** Multiple types of thermocouples supported */
typedef enum
{
MAX31856_TCTYPE_B = 0x00,//0b0000,
MAX31856_TCTYPE_E = 0x01,//0b0001,
MAX31856_TCTYPE_J = 0x02,//0b0010,
MAX31856_TCTYPE_K = 0x03,//0b0011,
MAX31856_TCTYPE_N = 0x04,//0b0100,
MAX31856_TCTYPE_R = 0x05,//0b0101,
MAX31856_TCTYPE_S = 0x06,//0b0110,
MAX31856_TCTYPE_T = 0x07,//0b0111,
MAX31856_VMODE_G8 = 0x08,//0b1000,
MAX31856_VMODE_G32 = 0x0C,//0b1100,
} max31856_thermocoupletype_t;
void write_max31856(uint8_t addr, uint8_t dt);
void read_max31856(uint8_t addr, uint8_t dt, uint8_t len);
float MAX31865_readTemp();
void set_thermocouple(uint8_t enable);
#endif
#include "MAX31856.h"
extern SPI_HandleTypeDef hspi2;
uint8_t TxBuffer[1] = {0};
uint8_t RxBuffer[1] = {0};
uint8_t data;
//------------------------------------------------
#define cs_reset() HAL_GPIO_WritePin(GPIOE, GPIO_PIN_15, GPIO_PIN_SET);
#define cs_set() HAL_GPIO_WritePin(GPIOE, GPIO_PIN_15, GPIO_PIN_RESET);
#define cs_strobe() cs_reset(); cs_set();
void write_max31856(uint8_t addr, uint8_t dt)
{
cs_strobe();
TxBuffer[0] = addr;
HAL_SPI_Transmit(&hspi2, (uint8_t*) TxBuffer,1,5000);
TxBuffer[0] = dt;
HAL_SPI_Transmit(&hspi2, (uint8_t*) TxBuffer,1,5000);
cs_reset();
}
void read_max31856(uint8_t addr, uint8_t dt, uint8_t len)
{
cs_strobe();
HAL_SPI_Receive(&hspi2,(uint8_t*)RxBuffer,1,5000);
addr = RxBuffer[0];
HAL_SPI_Receive(&hspi2,(uint8_t*)RxBuffer,1,5000);
dt = RxBuffer[0];
cs_reset();
}
void single_shot(void)
{
uint8_t status;
// Read config register
read_max31856(MAX31856_CR0_RREG, status, 1);
// Enable 1shot bit, and write back
status |= MAX31856_CR0_1SHOT;
write_max31856(MAX31856_CR0_WREG, status);
}
void autoConvert(uint8_t enable)
{
uint8_t status;
read_max31856(MAX31856_CR0_WREG, status, 1);
if (enable)
{
status |= MAX31856_CR0_AUTOCONVERT;
} else
{
status &= ~MAX31856_CR0_AUTOCONVERT;
}
write_max31856(MAX31856_CR0_WREG, status);
}
void set_thermocouple(uint8_t enable)
{
uint8_t status;
read_max31856(MAX31856_CR1_RREG , status, 1);
if (enable)
{
write_max31856(MAX31856_CR1_WREG , MAX31856_TCTYPE_T);
} else
{
write_max31856(MAX31856_CR1_WREG , MAX31856_TCTYPE_K);
}
//write_max31856(MAX31856_CR1_REG , MAX31856_TCTYPE_T);
}
float MAX31865_readTemp()
{
// Activate autoconversation
autoConvert(ON);
HAL_Delay(10);
// Perform a single conversion, and wait for the result
single_shot();
HAL_Delay(65);
// Read data from max31856 data registers
uint8_t buffer[2];
read_max31856(MAX31856_LTCBL_REG,(uint8_t)buffer, 2);
// Combine 2 bytes into 1 number, and shift 1 down to remove fault bit
uint16_t data = buffer[0] << 8;
data |= buffer[1];
data >>= 1;
// Calculate the temperature
float temp = (float) data;
return temp;
}
- Labels:
-
SPI
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-27 7:43 AM
Could you tell me? Where did you find these codes?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-27 7:45 AM
Because you need to write a code into while(1) file in the main.c
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-24 1:19 PM
If you solved the problem, can you share the program codes with me?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-24 1:19 PM
ozgurkorkmaz236@hotmail.com
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-24 1:22 PM
hangi fonksiyonları yazmamız gerekiyor while döngüsünün içine?