cancel
Showing results for 
Search instead for 
Did you mean: 

Manual for Std Peripheral Drivers for STM32?

ccassey
Associate
Posted on January 29, 2011 at 18:59

Manual for Std Peripheral Drivers for STM32?

2 REPLIES 2
Posted on May 17, 2011 at 14:23

www.st.com/stm32-discovery routes to

http://www.st.com/internet/evalboard/product/250863.jsp

Design Support

Software & Development tools - Firmware (Bottom of Page)

http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32vldiscovery_package.zip

Top level directory you'll find

stm32f10x-an3268_fw.chm

Now I'll note that the examples from the old library, included with Keil and IAR evals, might be a better starting point as there are more different code examples than for the VL. The VL only works at upto 24 MHz, so you'll have to watch that.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ccassey
Associate
Posted on May 17, 2011 at 14:23

Thanks clive1, but I already have that - it is the help for the VL Discovery firmware package, not the Standard Peripheral Library.  That is not included in the VL Discovery firmware package.  So does it exist, somewhere else?