2017-11-16 8:53 PM
i am facing the write and read issue in M95M02 EEPROM, i am follow the read write cycle as per data sheet.
but not write and read in EEPROM.
MCU: STM32F105RB.
my read write algorithm in below.
/************************************WRITE Algorithm******************************/
/**
* @brief Transmit a byte of data in blocking mode. * @param addr: Data addresh * @param ptr_dat: Pointer to data buffer * @retval HAL status */HAL_StatusTypeDef EEPROM_Byte_Write(uint8_t *ptr_dat, uint32_t addr){ HAL_StatusTypeDef status = HAL_OK; uint8_t temp = 0x00, *ptr_temp = '\0'; /* Send Write Enable Command */ CHIP_SEL_RESET(); // Chip select Low temp = (uint8_t)WREN; HAL_SPI_Transmit(&hspi1, &temp, 1, 10); HAL_Delay(10); CHIP_SEL_SET(); // Chip select High /* Send Write To Memory Array Command */ CHIP_SEL_RESET(); // Chip select Low temp = (uint8_t)WR; HAL_SPI_Transmit(&hspi1, &temp, 1, 10); /* EEPROM 24 Bit Addresh Send */ ptr_temp = (uint8_t *)&addr; HAL_SPI_Transmit(&hspi1, ptr_temp, 3, 10); /* Sending One Byte In EEPROM */ status = HAL_SPI_Transmit(&hspi1, ptr_dat, 1, 10); /* Send Write Disable Command */ temp = (uint8_t)WRDI; HAL_SPI_Transmit(&hspi1, &temp, 1, 10); CHIP_SEL_SET(); // Chip select High return status;}/*************************************************************************************/
/************************************READ Algorithm*******************************/
/**
* @brief Receive a byte of data in blocking mode. * @param addr: Data addresh * @param ptr_dat: Pointer to data buffer * @retval HAL status */HAL_StatusTypeDef EEPROM_Byte_Read(uint8_t *ptr_dat, uint32_t addr){ HAL_StatusTypeDef status = HAL_OK; uint8_t temp = 0x00, *ptr_temp = '\0'; /* Send Read To Memory Array Command */ CHIP_SEL_RESET(); // Chip select Low HAL_Delay(10); temp = (uint8_t)RD; HAL_SPI_Transmit(&hspi1, &temp, 1, 10); /* EEPROM 24 Bit Addresh Send */ ptr_temp = (uint8_t *)&addr; HAL_SPI_Transmit(&hspi1, ptr_temp, 3, 10); /* Receving One Byte From EEPROM */ status = HAL_SPI_Receive(&hspi1, ptr_dat, 1, 50);CHIP_SEL_SET(); // Chip select High
return status;}/*************************************************************************************/
2017-11-16 10:27 PM
Quick guess (no time to browse the spec) : after you finish writing, let NSS goes up, wait 10 msec, disable write protect, then read (verify).