2018-12-07 5:15 AM
Hello.
When I loaded the array into Flash (used const) It was displayed on the screen
But as soon as I use RAM to store the image it stops displaying, I see a black square
I also can not fill the color programmatically LTDC just does not react
2018-12-07 5:51 AM
What RAM?
The LTDC needs the data in the AXIM RAM
2018-12-07 6:49 AM
2018-12-07 7:23 AM
Thank you.
So I have to run an external SDRAM?
I was just creating an array (uint8_t image[100 * 100])
2018-12-07 7:26 AM
>>So I have to run an external SDRAM?
No
>>I was just creating an array (uint8_t image[100 * 100])
Pay attention to the memory region from which it gets allocated, review linker script or scatter file, and that it describes available memories properly, and that you direct allocations from the appropriate pools/sections.
2018-12-08 4:03 PM
I don't really understand.
Is it possible to put a variable in the desired area of memory without explicitly specifying an address?
I'd like the compiler to do it myself.
In linker script script there is
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
}
Do I need RAM_D1 or RAM_D2 or RAM_D3?
2018-12-08 5:54 PM
>>Do I need RAM_D1 or RAM_D2 or RAM_D3?
The AXIM SRAM is in the D1 Domain, so RAM_D1
>>Is it possible to put a variable in the desired area of memory without explicitly specifying an address?
Yes, you use an attribute directive, and let the compiler/linker do their respective jobs
Something like this would be GNU/GCC syntax with suitable section definitions in the .LD file
uint8_t __attribute__ ((section (".RAM_D1"))) image[100 * 100];
Example:
\STM32Cube_FW_H7_V1.3.0\Projects\NUCLEO-H743ZI\Examples\MDMA\MDMA_LinkedList\Src\main.c
2018-12-10 1:30 AM
Thank you.
I have a result.
I copied the linker script from the project "Mdma_linkedlist ".
I fill the square with white and black once a second and here's the result.
Perhaps I should just use an external SDRAM? It'll take time, but I'd have to do it anyway.