2025-12-08 8:23 AM - last edited on 2025-12-08 8:33 AM by Andrew Neil
HI all i have been working with LTDC to drive an external RGB parallel display . i made it working by placing the framebuffer inside internal RAM . i got output with good update speed. but when i try to incoperate FREERTOS with this project the output is gone . any one encountered such issues like this , any solution for this now? ;)
2025-12-08 8:31 AM - edited 2025-12-08 8:31 AM
An RTOS (any RTOS) is not really something that you can just bolt-on to an existing project - it is a fundamental change to the project architecture.
You'll need to do some debugging to find why your code is not working ...