2023-10-16 8:06 PM
I want to read Temperature data in register [20h,21h] , but the data I read are 0x00 , should I setting which register ?
2023-10-17 1:21 AM
Hello @KevinHSU,
Thank you for your question.
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-17 7:03 PM
Hellow Pierre
The FIFO_CTRL4 (0Ah) value is 0x30 , so ODR_T_BATCH_[1:0] is "11" , and I check the 1Eh still 0x00 .
Do you have another suggestion
thanks
2023-10-18 1:43 AM
Hello @KevinHSU,
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.