cancel
Showing results for 
Search instead for 
Did you mean: 

low accuracy for ADC1 on STM32F030R8-Nucleo

Benjamin Brammer
Senior II
Posted on June 09, 2018 at 14:28

Hey Guys,

I am using the ADC1 to sample A0 as a voltage input and A17 and A18 as temperature and VrefInt for Temperature and exact Vdda calculaion. So far my implementation works fine. I also calibrate the ADC everytime before I start the ADC. Datahandling is done via DMA in circular mode, so continous.

I also want to use the analog WatchDog to check wether my voltage on A0 is inside a specified range (0,8V - 3V). Sadly when I programm the lower and upper threshold value for the watchdog and try to test it with my laboratory power supply, The watchdog triggers from 2,7V not 3. When I compare the converted values I see some overshots in reading. As I am avagering my calculated values this is not bothering me, but for the accuracy of the WatchDog this is a problem.

Has anybody seen this kind of behaviour before? Am I doing something wrong, or forgot something? Or is this inherent since the integrated ADC is simply not very accurate?

For the thresholds I used the following formula: HT = 3V * 4095/3,3V and LT = 0,8V * 4095/3,3V

So I would be happy for any help

best regards

Benjamin

#analog-watchdog #adc #adc-accuracy
This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
Posted on June 19, 2018 at 13:47

Hey AvaTar,

sorry for my late reply but I had other stuff to attend to. I measured the Vdda on the board after the L1 ferrite bead with my oscilloscope and a one second sampling intervall. There Vp+ is 3,3525V and Vp- is 3,3213V so this seems good for me. The power supply is very accurate i.e. 2,52V PS is 2,5205 on my calibrated multimeter. Concerning the shottky diodes I don't see them in the schematics of the Nucleo64..

best regards

Benjamin

Posted on June 19, 2018 at 14:09

I forgott to write that there seems to be a conversion fault of 0,001742,,,V . So for example I put in 1V, measure 1V at the A0 Input of the ADC but get 0,998258.. as a conversion result this would mean I have about 35 LSBs error. This seems a little high or am I misunderstanding here something?

Maybe this fault is due to my cnversion equation? 

here it is:

                  Voltage.data = (float)((3.3 * (uint32_t) *VREFINT30_CAL_ADDR * tempVolt)/ (tempVref * 4095));

it's basically the suggestion from the manual..

best regards

Benjamin

Posted on June 19, 2018 at 14:15

but nevertheless the watchdog triggers at 0,84V allthoug I set it up for 0,799V at the lower end and at 2,99V at the upper end for a set threshold of 3V.

Posted on June 19, 2018 at 14:19

To be honest, I never really tried the AWD functionality of the F0 devices. Always used a software implementation (like you described), having the advantage of being adaptable e.g. for filtering, and portable to other platforms/devices.

Could be a matter of configuration settings, or settling time issues of the hardware. The AWD hardware supposedly consists of a DAC and a comparator.

Posted on June 25, 2018 at 17:08

Thanks so far for your help. I would say we keep it that way as everything is working fine without the AWD.

best regards

Benjamin