cancel
Showing results for 
Search instead for 
Did you mean: 

linux toolchain for smt32f4

bifrost
Associate II
Posted on June 04, 2012 at 10:55

Hi,

i'm new in the arm world, and i have bought a smt32f4 (maybe not so good for a kickstart, but i'll survive).

i'm compiling the gcc arm eabi toolchain, but i've also seen the Yargarto, is quite used here.

For my final project i need hard float, UART or USART, usb (for debug and data log), i2c, more in future SPI.

Will any of the 2 above toolchain support some library to speed up my development, or will i have to write everything from register?

#toolchain-linux
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
frankmeyer9
Associate II
Posted on June 04, 2012 at 11:50

The summon arm toolchain there supports the stm32f4:

http://www.triplespark.net/elec/pdev/arm/stm32.html

If I remember correctly, it sets up a preconfigured StdPeripheral_Library project template, that was copied over from the Atollic Lite toolchain, including the linker script and startup code.

I did some experimentation with it, and successfully compiled and ran both  softfp and hardfp code. As expected for a cmd line toolchain, you have to adapt the makefile yourself.

But mostly I use Crossworks, so I didn't get really deep into...

bifrost
Associate II
Posted on June 04, 2012 at 12:18

Thanks very much,

helpful link, it solve some problem building openODC separately (i've got some different error, anyway, but this should do the trick)!

Also a very good explanation of what come AFTER i will have a working toolchain.

bifrost
Associate II
Posted on June 05, 2012 at 09:45

int the end i'm using http://www.archlinux.org/packages/community/x86_64/arm-elf-gcc-base/;

i've GCC 4.7 and autoconf 2.69 who seems to be too much mainstream for the others toolchain, config and compilation give too much error.

Autoconf still give me some problem with st-link, but there is already an open issue.