2023-06-02 4:36 AM
I have two boards: STM32L4xx and STM32H7xxQ.
I use cubeAI 8.0.1 and tflite for a project in vision.
Having set all includes and settings, I successfully build and flash my code on the first board.
The second project uses the same include paths (exported from the first project -> imported), and the only differences must be: 1) board 2) USART port 3) CMSIS/Device
However, the same code fails to compile for the second board, resulting in:
undefined reference to `vtable for tflite::MicroErrorReporter'which looks like a linker issue.
Are there any special instructions for how to debug what is happening, and understand what caused the difference in compilation between the two projects?