Skip to main content
regmaster2
Associate II
November 9, 2010
Question

Lib PLL configuration wrong for F105?

  • November 9, 2010
  • 3 replies
  • 942 views
Posted on November 09, 2010 at 03:50

Lib PLL configuration wrong for F105?

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:14

    Perhaps you don't have the most current version of the library, or you have not defined the family/model correctly within the project/compiler settings.

    What is the exact/complete part number for the part you are using?

    Connectivity Line

    #define STM32F10X_CL

    -DSTM32F10X_CL
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    regmaster2
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 14:14

    Hi,

    I have V3.4.0 and had that problem with versions before, too.

    The code I posted is below a

    #ifdef STM32F10X_CL

    so my mc type should be defined correctly.

    I did it with -DSTM32F10X_CL in the makefile.

    regmaster2
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 14:14

    Has someone an STM32 from the Connectivity Line running correctly after initializing with the standard lib?