cancel
Showing results for 
Search instead for 
Did you mean: 

[Layout] Ground plane recommendation for STM32 on BMS board

ytshin0877
Associate

 

Context (brief):

  • Board: BMS that charges/discharges cells at 1–2 A

  • MCU: STM32G474RET6 using HSI, 3× ADC, 1× DAC, USB FS (D+, D−), a few GPIOs.

  • Constraint: Battery sense node carries an unavoidable ~20 MHz component from an external stim source (cannot eliminate at source).

  • Goal: Accurate voltage sensing while keeping digital/USB activity and power-stage di/dt from polluting ADC/DAC/reference.

What I need advice on (grounding only):

  1. Single solid plane vs split AGND/DGND:

    • For STM32 with VSSA/VDDA and VSS/VDD, is the consensus to use one continuous GND plane (no hard moat) with functional partitioning—or do you still recommend a true AGND/DGND split in this use case (1–2 A BMS + ~20 MHz on the measured node)?

    • If “single plane,” where do you prefer the AGND focus/tie—directly under/next to VSSA/VREF+ (shortest loop) versus a separate star just for the analog front end?

  2. If I were to have two separte ground plane

    1. What component should I connect to AGND, and DGND?: My assumption was that since BMS board ground has lots of current(Charging/Discharging current flowing+ 20MHz signal), I wanted to separte ground for ADC and all the peripherals for the MCU. 
    2. Could you recommend the best strategy for implementing this MCU collaborated and implmented in the one PCB together?

Thank you in advance 

 

I would really appreciate any help regarding this layout recommendation

0 REPLIES 0