cancel
Showing results for 
Search instead for 
Did you mean: 

Kardware Key / Button debouncing with one-puls mode of general purpose timers

mrupprath
Associate II
Posted on March 17, 2013 at 14:32

Hello;

i have checked and tried the one -pulse example of the standard periheral library.

In the example The timer uses one channel as input (ch1) and one chanel (ch2) asl output for the pulse.

As a result a can use the one shot signal at ch2 as debounced signal / or the coressponding interupt trigger.

It works fine but it seems that i need 1 Timer to debounce 1 Inbut button.

One Timer has 4 channels my question is if it is possible to debounce more than one input button with a single timer ?

For example : is it possible to trigger two (four) independent one pulses by using ch1 and ch3 as inputs and ch2 and ch4 as outputs.

Or to use all channels as inputs and use the outputcompare register events as triggers ''input 1,2,3,4 are debounced''.

Thanks in advance.

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
emalund
Associate III
Posted on March 18, 2013 at 19:15

 if it is possible to debounce more than one input button with a single timer ?

as many as you want

answered in another thread

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Debouncing%20interrupts&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx&currentviews=142]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex%5fmx%5fstm32%2fDebouncing%20interrupts&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex%5Fmx%5Fstm32%2FAllItems%2Easpx&currentviews=142