cancel
Showing results for 
Search instead for 
Did you mean: 

Jump from Openbootloader to the Application

j_filipe
Associate III

Greetings! 
So, I used the OpenBootloader project, and then flashed a GPIO_IOToggle firmware in other area of the flash, close to the example in the video Introduction to Open Bootloader, Part 3: Loading an Application.  In that example the CubeProgrammer flashes through the DFU and check "run after programming". When I unplug the board and turn it back on, the OpenBootloader starts (as expected). 
What I want to do is, as soon as I flash the application, when I turn off the board and turn it on again, the application starts to run and not the bootloader, OR, it starts the bootloader, it checks if there's any application installed, and if yes, it jumps to the application immediately. 
Any clue on how to do that?
Thank you! 

0 REPLIES 0