2018-03-08 7:28 AM
Hi,
I've a problem with the jitter of my program on STM32L476.
First of all, I'm introduced you my project.
A signal TLL with a frequency of 1KHz to 50 KHz must be multiplied by a sinusoide or square analogique signal (10Hz to 1KHz) like a AM modulation. Then with the DAC of STM32 a results could be send in analogique format.
at the beginning I'm use a DMA for the ADC/DAC and a callback function trig by timer 6 (sampling Time 100 Khz).
In a call back function I'm get the state of the TTL and multiplied by the results of ADC (result *1 if the TTL state was SET or result *-1 if the results state is RESET), then I get the result in the DAC.
When I look the result with an osciloscope I see a 8 µs jitter and the frequency results is so bad especially near 50 Khz. period for 50Khz is 20 µs so sometime I see 35 KHz and sometime 80 KHz.
So I have modified my code like that. I made a new extern interuption on signal TTL and change the state of a variable 1 then -1. I use freeRTOS and give the high priority to the EXTI interupt. In a callback TIMER 6 i use the result of the ADC multiplied by the variable 1 or -1.
When I look the result with an osciloscope I see a 100ns jitter for the EXTI interrupt and always 8 µs jitter for the final results.
So my question is what is the minimal jitter I could have for my project?
I don't know really freeRTOS and i do'nt understand why i can't get a prioity value less than 5. This is a probem because i want the maximum priority to the EXTI interrupts to reduced the jitter.
Can I do like that:
only one interruption EXTI on signal TTL (between 1 to 50 Khz).
in the function of EXTI :
I manually start the DAC with the value of ADC( The first conversation could be wrong but it doesn't matter)
Then I manually START ADC (one sample)
I change the state of a variable example stateTTL = StateTTL * -1 to change 1 in -1 or -1 in 1.
I multiplied the value of ADC by stateTTL.
I think when I do like that I have the jitter of only the EXTI interrupts + the DAC jitter isn't it?
I want a precison of 50 Hz at 50KHz so I must have a global jitter less than 20ns. It is Possible?
Thank you for your answear.
here i attached a schema
2018-03-09 9:45 PM
I am thinking that the SAI interface would offer clean Jitter free analogue. since that is the primary function of SAI
I guess that requires extra circuitry.to convert it to an actual analog signal.
You have 2x SAIs on board this chip...
I guess you could use one as the analogue receiver and one as the transmitter,
but your latency may blow out,
how much latency can you tolerate ?