Skip to main content
TChri.2
Visitor II
April 9, 2021
Question

It is possible to use 16 slots with a bit depth of 24 bit with the SAI module

  • April 9, 2021
  • 0 replies
  • 467 views

Hi ST!

I would like to use 16 slots with a bit depth of 24 bits with the SAI module..

The problem is that the frame length is limited to 256, meaning I can't respect the mandatory condition which is that Number of slots * slot size <= Frame length..

This means that I can only use 10 slots (256/24=10.666)..

Is there away around this? Or is it only possible to use 16 slots with a bit depth of 16 bits?

This topic has been closed for replies.