2016-03-14 9:12 AM
I've been having trouble with getting the SysTick interrupt to trigger in a simple program using the standard peripheral library. The code should just pulse an LED every time the SysTick interrupt fires, but instead it just sits in the main() loop and never toggles the GPIO.
#include ''stm32f0xx.h''
GPIO_InitTypeDef GPIO_InitStruct;
NVIC_InitTypeDef NVIC_InitStruct;
void init()
{
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStruct);
NVIC_InitStruct.NVIC_IRQChannel = SysTick_IRQn;
NVIC_InitStruct.NVIC_IRQChannelPriority = 0;
NVIC_Init(&NVIC_InitStruct);
SysTick_CLKSourceConfig(SysTick_CLKSource_HCLK_Div8);
}
void LED_On()
{
GPIOA->BRR = GPIO_Pin_6;
}
void LED_Off()
{
GPIOA->BSRR = GPIO_Pin_6;
}
int main()
{
init();
LED_Off();
for(;;);
}
void SysTick_Handler()
{
LED_On();
LED_Off();
}
Am I missing something obvious that's needed to set up the SysTick interrupt handler? I've been looking around for a while and I haven't seen something other people are doing with the standard peripheral library that I'm not.
Thanks for any help.
2016-03-14 10:00 AM
If you can see a nS led blink. I can't. And most humans as well I think.
2016-03-14 11:28 AM
I'm measuring the pin with a scope
2016-03-14 1:03 PM
Using a .CPP file?
Using a debugger?2016-03-14 1:17 PM
Nope, just C files. I'm programming the board with an ST-Link and debugging over that using GDB. When I set breakpoints in the SysTick ISR they never get triggered.
I know that the GPIO/etc is correct because when I modify main() to readvoid main()
{
init();
for(;;)
{
LED_On();
LED_Off();
}
}
then the pin does toggle correctly (albeit rather slowly, only ~188KHz which seems slow given that the system_stm32f0xx.c file from the discovery board software library should be setting the system clock to 48MHz).
2016-03-14 1:28 PM
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
2016-03-14 1:33 PM
Don't use the NVIC_Init, this is a System Handler, not an IRQ
After selecting the clock source, you must actually configure and enable the SysTickSysTick_Config(SystemCoreClock / 1000); // 1ms (1000 times a second)2016-03-14 2:11 PM
That did it, thanks! Although when I comment out the NVIC_Init portion it stops working, are you sure that part isn't required?
2016-03-14 2:18 PM
Yeah, pretty sure
STM32F0xx_StdPeriph_Lib_V1.5.0\Projects\STM32F0xx_StdPeriph_Examples\SysTick\SysTick_Example\main.c