cancel
Showing results for 
Search instead for 
Did you mean: 

Is there going to be a pin compatible 216 BGA for H7?

bassetteporn11
Associate II

STM32H7 should be pin compatible version of STM32F777 and STM32F479 with BGA216.

Or there should be an H4 running @ 400 Mhz.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
AVI-crak
Senior

This makes no sense, they have a different set of peripherals.

bassetteporn11
Associate II

stm32f777 AND F469/79 ARE PIN TO PIN COMPATIBLE, H7 has only MDMA peripheral.

It has the jpeg engine, everything, double precision, etc.

There should an H4 then BGA216.

Leaving the best package out and claiming to be pin compatible.

Who would ever choose a 176 BGA with .65mm garbage routing over 240 .8mm easy routing.

ROFL? Hello...