Question
STM32L4 ADC+DMA how to get an interrupt when the buffer is filled?
HI, i am using STM32L476RG and need to acquire data at 1.5MSPS in a buffer, size 2048. Everything is working however i cant see how to get an interrupt once the buffer is filled.
I thought the TC flag could be used but when i check in the DMA interrupt i find this function : HAL_DMA_IRQHandler(AdcHandle.DMA_Handle); which it totally managed by the HAL, so i wonder how to get a flag or an interrupt once the buffer is fileld, because i will have to change the buffer in order to allow continuous acquisition while the filled buffer is processed with DSP instructions.
Thanks