cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a waY to provide a Timers external Clock Signal on CH1, but only if CH2 is Active?

AFied.1
Associate III

Hi,

I would like to provide / route a Timers external Clock Signal to CH1 pin, but only if CH2 is in Active state.

So that it acts kinda like a AND Gate.​

Is this possible? If so, how? Is there a sample somewhere I can have a look at?​

greetings and thanks,

André​

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

Not quite so. What can be done is to input external clock through TIMx_ETR and gate the timer by the slave-mode controller in Gated mode, controlled from CH1 or CH2.

JW