cancel
Showing results for 
Search instead for 
Did you mean: 

Is the TRNG of the STM32 L562RET6 also comform to the AIS31 standard?

SWans.1
Associate

Your microcontroller STM32 L562RET6 claims NIST SP800-90B conformity.

Does this TRNG also fit the criteria of the functionality class PTG.2 in the document

"A proposal for: Functionality classes for random number generators" [1]

Is the TRNG also comform to the AIS31 standard?

[1] https://www.bsi.bund.de/SharedDocs/Downloads/DE/BSI/Zertifizierung/Interpretationen/AIS_31_Functionality_classes_for_random_number_generators_e.pdf?__blob=publicationFile&v=1

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @SWans.1​ ,

Welcome to the STM32 Community :smiling_face_with_smiling_eyes:

STM32L5 TRNG should be compliant to AIS31 PTG.2 class, but it has not been through the certification process yet.  

Please mark my answer as best by clicking on the "Select as Best" button if it fully answered your question. This will help other users find this answer more quickly.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @SWans.1​ ,

Welcome to the STM32 Community :smiling_face_with_smiling_eyes:

STM32L5 TRNG should be compliant to AIS31 PTG.2 class, but it has not been through the certification process yet.  

Please mark my answer as best by clicking on the "Select as Best" button if it fully answered your question. This will help other users find this answer more quickly.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Thanks.