2022-04-29 12:54 AM
2022-04-29 12:54 PM
They're not fully compatible, but if you are using the subset of the features available to both, the binary will work.
At a quick glance, looks like USB is the only thing on the L475 that isn't on the L471. So as long as you're not using that, it'll work.
Otherwise, there are no drawbacks of using a binary made for another chip in this case. Might want to verify pinout as well.
2022-05-01 09:12 AM
Hello,
Thank you for this response. I am happy to hear that.
Have a nice day,
À bientôt,
Victor