cancel
Showing results for 
Search instead for 
Did you mean: 

Is STM32H725 VTOR bit assignments is not correspond ARM7M arcitecture?

Aleks
Associate III

Hi!

ST manual PM0253:

[31:9] TBLOFF Vector table base offset field. It contains bits [29:7] of the offset of the table base from the bottom of the memory map.

[8:0] - Reserved

Arm v7-M Architecture Reference Manual:

Bits[31:7] of the vector table address.

Older documentation describes this field as the vector table address offset. The description

in this manual clarifies the use of this register.

Bits[6:0] - Reserved

Is there wrong assignment description in PM0253?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Super User

For STM32H7 the vectors address must be aligned at least on 0x400

Learned in a hard way ((

See at end of this thread. @Piranha​ explains it.

Yes, on M7 VTOR is the vector table base address - including the lower zero bits - because of alignment requirement.

View solution in original post

3 REPLIES 3
Pavel A.
Super User

For STM32H7 the vectors address must be aligned at least on 0x400

Learned in a hard way ((

See at end of this thread. @Piranha​ explains it.

Yes, on M7 VTOR is the vector table base address - including the lower zero bits - because of alignment requirement.

It depends on how the ARM IP builds​ based on the number of interrupt used by the NVIC, unused inputs are optimized away.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Aleks
Associate III

Great thanks for additional material.