Skip to main content
Associate III
November 25, 2021
Solved

Is it possible to use multiple functions on a single pin on STM32U5?

  • November 25, 2021
  • 2 replies
  • 2933 views

According to the RM, I think that it is possible to use multiple analog functions on a single pin.

Can we do the same with digital pins? What I would need is to put a timer channel (as input) and an external interrupt input on the same pin.

This topic has been closed for replies.
Best answer by TDK

In general, you can only use one peripheral (alternate function) at a time on a pin. However, EXTI operates independently from the peripherals, so you can use this independently. HAL doesn't support this, but it can be set up in code manually.

So yes, you can enable an EXTI interrupt on a pin while still using it as a digital input/output/AF.

2 replies

TDK
TDKBest answer
November 25, 2021

In general, you can only use one peripheral (alternate function) at a time on a pin. However, EXTI operates independently from the peripherals, so you can use this independently. HAL doesn't support this, but it can be set up in code manually.

So yes, you can enable an EXTI interrupt on a pin while still using it as a digital input/output/AF.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate III
November 25, 2021

That is a good feature

Thank you