cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to upload/disassemble STM32 Flash?

rlongdon
Associate II
Posted on February 05, 2009 at 18:48

Is it possible to upload/disassemble STM32 Flash?

1 REPLY 1
rlongdon
Associate II
Posted on May 17, 2011 at 13:02

A recent hardware failure of my ''super secure'' IronKey Thumb Drive left me with months of work lost. I had backed up this work onto multiple PC's using the IronKey secure backup program. Now I am learning from IronKey that there are some issues that will not allow this encrypted backup to be restored!

I have an STM32F103VBT6 that contains code in it's flash. Is there anyway to extract and disassemble this code to aid in cutting my losses. The flash is not locked. I use a Segger J Link to program and debug.

Any thoughts?

Thanks and Kind regards,

Russ Longdon