cancel
Showing results for 
Search instead for 
Did you mean: 

Is it okay to connect a 25v wire on an A0 pin to The STM32F072RB Dev board?

JS.4
Associate

While testing the data line, I have connected a wire to an A0 pin which gives 25v on full throttle signal. After dumping the code can't get any output as expected and found few registers were heating up.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

> Is it okay to connect a 25v wire on an A0 pin to The STM32F072RB Dev board?

No.

JW

TDK
Super User

The Absolute Maximum Values for pins are listed in the datasheet. In most cases, 5V is the max. In some cases, 3.3V (or operating voltage) is the max.

If you feel a post has answered your question, please click "Accept as Solution".
Uwe Bonnes
Chief

An 5 V on 5-Volt tolerant pins is also only allowed on a powered device!