Skip to main content
Associate III
May 14, 2025
Question

Interrupt Vector Table

  • May 14, 2025
  • 6 replies
  • 4102 views

Hello,
As per CM4 guide and TRM of Nucleo f446re,interruot vector table is array of function pointers and each pointer holds the entry address(initial address) of each IRQ_handler, Where interrupt IRQ_number is used for indexing.

While debugging I failed to observe the intial address of teh reset handler and USART2_Handler at location 0x0000 0004 and 0x0000 00DC respectively.Please find the samething in attachments.Address fo the IRQ_handlers are available in expressions window snapshot and actuall value stored at location 0x0000 0004 and 0x0000 00DC is not matching.
Am I missing something here?
I am just verifying my understanding -->"At each location in IVTable,address oif IRQ handlers should be ther (&<IRQ_Handler_Name>Screenshot 2025-05-14 222309.png

 

Screenshot 2025-05-14 222359.png

 

Screenshot 2025-05-14 222411.png

 

"

6 replies

Tesla DeLorean
Guru
May 14, 2025

Hard to discern from the presentation.

Perhaps the built code and the code on the device aren't current / coherent.

Make sure the build complete, and the code delivered / verified. Check Release vs Debug build

Check the .MAP file, perhaps OBJDUMP the .ELF

What function is at 0x08000530 ? The ODD version is jump the +1 indicating the code is THUMB/16-BIT

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
KnarfB
Super User
May 14, 2025

The renderings seem to be in the wrong endianess, so 690A0008 reads 0x08000A69 (match!) and the other handler seems to be one word to the left: 1D050008 -> 0x0800051D. The least significant bit indicates a branch to thumb mode code.

hth

KnarfB  

Associate III
May 15, 2025

Thanks @KnarfB ,

Thats sounds right.how to change the endianess

KnarfB
Super User
May 15, 2025

in the Memory View: New Renderings... -> Hex Integer 

hth

KnarfB

 

Associate III
May 15, 2025

Hi knarfb,

Didn't get thing.could u please eloborate

Associate III
May 20, 2025

Hi, could you explain a bit more on that

Tesla DeLorean
Guru
May 20, 2025

That there is a configuration item that controls how the hex data is presented in the memory dump. It doesn't change what's in memory. 

You could also print out the vector table as an array of 32-bit unsigned into. Use the serial console and printf() to format as desired. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate III
May 20, 2025

Hi,

Ok I got it.what to assign user defined function as an interrupt handler to some ISR.

Currently for all interrupts,there is already handler names declared as weak functions.

 

Best RGS,

Alex

Associate III
May 23, 2025

Hi,

I got it.as youa re asking to use same function names declared in startup file.I tried it si working .But  I am looking for soltion where I have define some function funcHandler() and It need to attach this on interruptVectorTable.for example at 0x000000DC(Loc at IVT) i,e, &funcHandler needs to be placed at 0x000000DC.
How to Achive this.
I tried to use pointer also.
uint32_t *p;

p=(uint32_t *)(0x000000DC);

*p=(uint32_t)&funcHandler;

while debugging,value didnt change

 

KnarfB
Super User
May 23, 2025

this area is flash memory and you cannot write to it like writing to RAM. You may however relocate the entire vector table to SRAM using SCB->VTOR.

 

Associate III
May 24, 2025

Thanks knarfb, I git the answer.thanks for the support an precise answer.

You may close this ticket