2009-05-24 2:04 AM
Interrupt vector handler locations in raisonance tool chain ?
2011-05-17 4:12 AM
Hi all, I'm slowly picking up C, and getting to like it a ''bit'' even :)
However, I'm experiencing frustration in an area that I think most of you have already solved: Interrupts. The interrupts seem to be partially covered with code segments for enabling, disabling etc in each pheripheral *.C file, but I can't find/don't understand where the interrupt vector table lines up with the actual handlers. Some of the older builds seem to use a STM32f10xit.h and STM32f10xit.c file for the task, but the newer STM libraries are harder to understand. My main files are: main.c, which includes: stm32f10x_lib.h and stm32f10x_conf.h the lib file includes a map file, conf allows it to include a type file and cortexm3_macro.h I use the gpio file as well. My program runs, but I want to expand it, and use interrupts for much of the I/O maintainence. Can anybody explain what I'm missing please ? :o thanks in advance, Graham.