2009-06-08 11:24 PM
Interrupt priority grouping field, NVIC_PriorityGroup
2011-05-17 03:16 AM
Hi,
The description and number of NVIC_PriorityGroup constants in the firmware library does not match the PRIGROUP field description in the Cortexâ„¢-M3 Technical Reference Manual. Is there a bug? Thanks, Olek2011-05-17 03:16 AM
Dear olek ,
Could you give more details what do you mean by does not match ? The Cortexâ„¢-M3 Technical Reference Manual is a generic document from ARM implementing up to 241 external Interrupts in the micro & up to 8-bits of priorities. In STM32F10x we have 43 external interrupts (different from the Cortex-M3 core) and only 16 levels (4-bit) of priorities are implemented. Which is enough to handle all the Interrupts priorities levels. Implementing all bits is a waisting of the silicon area. ;-) Regards, STOne-32.2011-05-17 03:16 AM
Dear STOne-32,
Thank you very much for your clarification. It is exactly what I was looking for. The UM0306 manual actually states that there are 16 programmable priority levels. However, it does not mention that only values from 7 to 3 are accepted by the PRIGROUP field in the Application Interrupt and Reset Control Register due to this limitation. Thank you again. Best regards, Olek2011-05-17 03:16 AM
Hi,
At least for me it was a little confusing that ST naming (in that matter) is opposite to ''official'' ARM naming. I mean that ST names priority group using number of bits assigned for preempt priority field and ARM uses names coming from exact value of PRIGROUP. ST: NVIC_PriorityGroup_0 - 0 bits for pre-emption priority 4 bits for subpriority, defined value of PRIGROUP 7 ARM: PRIGROUP 7 - 0.8 indicates no pre-emption priority, eight bits of subpriority Descriptions match but their names not. Regards,