cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt on output PWM

instantni
Associate II
Posted on September 05, 2014 at 05:28

I'm trying to set up interrupt on falling/raising edge on output PWM line. This line drives LEDs (through TI LED driver chip). The reason why I need this is that the TI chip would report issues on a different pin but this pin is synchronized with PWM line - one comms bit per PWM signal.

I've tried to configure update interrupt but the handler never gets triggered. Any ideas why?

Here's my code

#define LED_GPIO_PORT             GPIOA

#define LED_GPIO_RCC              RCC_APB2Periph_GPIOA

#define LED_GPIO_PWM_PIN          GPIO_Pin_11

#define PWM_FREQUENCY_Hz 3000

#define PWM_MAX_DUTY_CYCLE    40 // 40%

#define LED_TIMER TIM1

#define LED_TIMER_RCC RCC_APB2Periph_TIM1

void LEDInit( void )

{

    ....

    GPIO_InitTypeDef GPIO_InitStructure;

    TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

    NVIC_InitTypeDef NVIC_InitStructure;

    TIM_OCInitTypeDef  TIM_OCInitStructure;

    // turn on clocks

    RCC_APB2PeriphClockCmd( LED_GPIO_RCC | LED_TIMER_RCC, ENABLE );

    NVIC_InitStructure.NVIC_IRQChannel = TIM1_UP_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 3;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    /* TIM IT enable */

    TIM_ITConfig( LED_TIMER, TIM_IT_Update, ENABLE );

    TIM_Cmd( LED_TIMER, ENABLE );

    GPIO_InitStructure.GPIO_Pin = LED_GPIO_PWM_PIN;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_Init( LED_GPIO_PORT2, &GPIO_InitStructure );

    TIM_TimeBaseStructure.TIM_Period = (SystemCoreClock/2) / PWM_FREQUENCY_Hz - 1;

    TIM_TimeBaseStructure.TIM_Prescaler = 0;

    TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;

    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_CenterAligned1;

    TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;

    TIM_TimeBaseInit( LED_TIMER, &TIM_TimeBaseStructure );

    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

    TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset;

    TIM_OCInitStructure.TIM_Pulse = period - dutyLength;

    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;

    TIM_OC4Init( TIM1, &TIM_OCInitStructure );

    TIM_OC4PreloadConfig( LED_TIMER, TIM_OCPreload_Enable );

    TIM_CtrlPWMOutputs( LED_TIMER, ENABLE );

}

void TIM1_UP_IRQHandler(void)

{

    if (TIM_GetITStatus( LED_TIMER, TIM_IT_Update ) != RESET)

    {

// do something here

        TIM_ClearITPendingBit( LED_TIMER, TIM_IT_Update );

    }

}

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
waclawek.jan
Super User
Posted on September 05, 2014 at 09:33

And does the PWM pin pulse?

JW
instantni
Associate II
Posted on September 09, 2014 at 12:19

Yes, the LEDs are working fine, I can see the PWM on the scope as well...

Posted on September 09, 2014 at 14:22

Are you using C++ (.cpp)?

I perhaps would have ordered things differently, and assigned all the fields in TIM/GPIO structures.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
instantni
Associate II
Posted on September 09, 2014 at 22:15

No, just C (using old CrossStudio). Is the order important? I'll try to fill all the fields.

Thanks

Posted on September 10, 2014 at 03:23

I'm going to guess this is an STM32F1 device.

How are you determining the interrupt is not occurring? Could you perhaps toggle a GPIO or something?

The other thing to look at would be your startup_stm32f1xx_xx.s file and make sure you have the interrupt vector described there. The C, whilst incomplete, looks like it should probably work.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..