cancel
Showing results for 
Search instead for 
Did you mean: 

interrupt in overflow event of timer in up/down mode

abdelhadi
Associate
Posted on August 02, 2016 at 10:58

Hello,

I use a nucleo stm32f401RC Evaluation Board for the regulation of a boost converter and I need to generate the interruption on the ON half-signal of PWM and I need also synchronize the conversion of 3 channel of the  adc using DMA with this interruption, to do this I set the timer 3 on the way up / down and I activated the global interruption of this timer.

My first problem is that the interrupt generated in the overflow and underflow of the timer, I want an interrupt only on the overflow.

Second problem, I generate a  event output of timer 3 for connecting it with the input trigger of the DMA and I got the same problem, the conversion is done on the overflow and underflow.

int main(void)

{

  HAL_Init();

  /* Configure the system clock */

  SystemClock_Config();

  /* Initialize all configured peripherals */

  MX_GPIO_Init();

  MX_DMA_Init();

  MX_ADC1_Init();

  MX_TIM1_Init();

  MX_TIM3_Init();

  MX_TIM4_Init();

      HAL_TIM_Base_Start_IT(&htim3);

 

      HAL_TIM_PWM_Start(&htim3,TIM_CHANNEL_1);

      TIM3->CCR1=0;

       HAL_TIM_PWM_Start(&htim13,TIM_CHANNEL_2);

       TIM3->CCR2=0;

/

  while (1)

  {

  }

}

/* TIM3 init function */

void MX_TIM3_Init(void)

{

  TIM_ClockConfigTypeDef sClockSourceConfig;

  TIM_SlaveConfigTypeDef sSlaveConfig;

  TIM_MasterConfigTypeDef sMasterConfig;

  TIM_OC_InitTypeDef sConfigOC;

  htim3.Instance = TIM3;

  htim3.Init.Prescaler = 0;

  htim3.Init.CounterMode = TIM_COUNTERMODE_CENTERALIGNED1;

  htim3.Init.Period = 10000;

  htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

  HAL_TIM_Base_Init(&htim3);

  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;

  HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig);

  HAL_TIM_PWM_Init(&htim3);

  sSlaveConfig.SlaveMode = TIM_SLAVEMODE_GATED;

  sSlaveConfig.InputTrigger = TIM_TS_ITR0;

  HAL_TIM_SlaveConfigSynchronization(&htim3, &sSlaveConfig);

  sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;

  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

  HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig);

  sConfigOC.OCMode = TIM_OCMODE_PWM1;

  sConfigOC.Pulse = 0;

  sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

  sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

  HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1);

  HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2);

  HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_3);

  HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_4);

}

/* ADC1 init function */

void MX_ADC1_Init(void)

{

  ADC_ChannelConfTypeDef sConfig;

    /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) 

    */

  hadc1.Instance = ADC1;

  hadc1.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV2;

  hadc1.Init.Resolution = ADC_RESOLUTION12b;

  hadc1.Init.ScanConvMode = ENABLE;

  hadc1.Init.ContinuousConvMode = ENABLE;

  hadc1.Init.DiscontinuousConvMode = DISABLE;

  hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_FALLING;

  hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T3_TRGO;

  hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;

  hadc1.Init.NbrOfConversion = 4;

  hadc1.Init.DMAContinuousRequests = ENABLE;

  hadc1.Init.EOCSelection = EOC_SINGLE_CONV;

  HAL_ADC_Init(&hadc1);

    /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 

    */

  sConfig.Channel = ADC_CHANNEL_1;

  sConfig.Rank = 2;

  sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;

  HAL_ADC_ConfigChannel(&hadc1, &sConfig);

    /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 

    */

  sConfig.Channel = ADC_CHANNEL_3;

  sConfig.Rank = 3;

  HAL_ADC_ConfigChannel(&hadc1, &sConfig);

    /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 

    */

  sConfig.Channel = ADC_CHANNEL_4;

  sConfig.Rank = 4;

  HAL_ADC_ConfigChannel(&hadc1, &sConfig);

}

void TIM3_IRQHandler(void)

{

  /* USER CODE BEGIN TIM3_IRQn 0 */

  /* USER CODE END TIM3_IRQn 0 */

  HAL_TIM_IRQHandler(&htim3);

  /* USER CODE BEGIN TIM3_IRQn 1 */

  HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_8);

    TIM4->CCR1=5000;//duty_reg;

  /* USER CODE END TIM3_IRQn 1 */

}

in attachement  a screenshot  of the PWM and GPIO togled in the IRQ handler

Any help would be much appreciated!

Many thanks,
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on August 31, 2016 at 16:06

Hi bou.abdel

I suggest you refer to the

http://www.st.com/content/ccc/resource/technical/document/application_note/group0/91/01/84/3f/7c/67/41/3f/DM00236305/files/DM00236305.pdf/jcr:content/translations/en.DM00236305.pdf

(General-purpose timer cookbook) and its associated firmware (

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-software/x-cube-timcooker.html

). It contains some examples that may be helpful for you, mainly the ones using DMA.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.