cancel
Showing results for 
Search instead for 
Did you mean: 

internal sram read and write

bilal
Associate II
Posted on March 25, 2013 at 08:53

hi

 

i am new to stm32f4. i want to read and write data to the internal sram (4kb). i am using mdk arm for compiling c code.

 

 

regards

 

 

5 REPLIES 5
Posted on March 25, 2013 at 12:54

The battery backed up regions?

I'd imagine you'd have to enable the PWR/BKP domain, and clocks (AHB1 BKPSRAMEN), and simply cast a structure or pointer to the memory region (0x40024000), then access it like you would any other memory.

You understand how to cast to fixed addresses in C, right?

uint8_t *BKPRam = (uint8_t *)0x40024000;

I don't think I'd involve the compiler with generate data for this region, but rather code the application to check it's validity, and copy in some default values. I'd use a structure to manage this space.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 25, 2013 at 23:09

''i am new to stm32f4''

Do you have experience with any other microcontrollers?

 

 

Do you have experience with programming in any other environment(s)?

 

bilal
Associate II
Posted on March 27, 2013 at 20:10

thank u clive for ur response 

i just got sram working, read and write data on sram

i have connected VBAT 3.3V cell, and using an LSI, but when i switch off the power that is controller running on VBAT, sram does not retain value

i am posting the main function of code that i picked from stm32eval project examples

void RTC_Config(void)

{

  /* Enable the PWR clock */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);

  /* Allow access to RTC */

  PWR_BackupAccessCmd(ENABLE);

    

#if defined (RTC_CLOCK_SOURCE_LSI)  /* LSI used as RTC source clock*/

/* The RTC Clock may varies due to LSI frequency dispersion. */

  /* Enable the LSI OSC */ 

  RCC_LSICmd(ENABLE);

  /* Wait till LSI is ready */  

  while(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET)

  {

  }

  /* Select the RTC Clock Source */

  RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI);

  

  SynchPrediv = 0xFF;

  AsynchPrediv = 0x7F;

#elif defined (RTC_CLOCK_SOURCE_LSE) /* LSE used as RTC source clock */

  /* Enable the LSE OSC */

  RCC_LSEConfig(RCC_LSE_ON);

  /* Wait till LSE is ready */  

  while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET)

  {

  }

  /* Select the RTC Clock Source */

  RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);

  

  SynchPrediv = 0xFF;

  AsynchPrediv = 0x7F;

#else

  #error Please select the RTC Clock source inside the main.c file

#endif /* RTC_CLOCK_SOURCE_LSI */

  

  /* Enable the RTC Clock */

  RCC_RTCCLKCmd(ENABLE);

  /* Wait for RTC APB registers synchronisation */

  RTC_WaitForSynchro();

  /* Write to the first RTC Backup Data Register */

  RTC_WriteBackupRegister(RTC_BKP_DR0, FIRST_DATA);

  /* Display the new RCC BDCR and RTC TAFCR Registers */

//  LCD_UsrLog (''RTC Reconfig \n'');

//  LCD_UsrLog (''RCC BDCR = 0x%x\n'', RCC->BDCR);

//  LCD_UsrLog (''RTC TAFCR = 0x%x\n'', RTC->TAFCR); 

  /* Set the Time */

  RTC_TimeStructure.RTC_Hours   = 0x08;

  RTC_TimeStructure.RTC_Minutes = 0x00;

  RTC_TimeStructure.RTC_Seconds = 0x00;

  /* Set the Date */

  RTC_DateStructure.RTC_Month = RTC_Month_March;

  RTC_DateStructure.RTC_Date = 0x18;  

  RTC_DateStructure.RTC_Year = 0x11; 

  RTC_DateStructure.RTC_WeekDay = RTC_Weekday_Friday; 

  /* Calendar Configuration */

  RTC_InitStructure.RTC_AsynchPrediv = AsynchPrediv;

  RTC_InitStructure.RTC_SynchPrediv =  SynchPrediv;

  RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24;

  RTC_Init(&RTC_InitStructure);

  

  /* Set Current Time and Date */

  RTC_SetTime(RTC_Format_BCD, &RTC_TimeStructure);  

  RTC_SetDate(RTC_Format_BCD, &RTC_DateStructure); 

  /* Configure the RTC Wakeup Clock source and Counter (Wakeup event each 1 second) */

  RTC_WakeUpClockConfig(RTC_WakeUpClock_RTCCLK_Div16);

  RTC_SetWakeUpCounter(0x7FF);

  

  /* Enable the Wakeup Interrupt */

  RTC_ITConfig(RTC_IT_WUT, ENABLE);

  /* Enable Wakeup Counter */

  RTC_WakeUpCmd(ENABLE); 

/*  Backup SRAM ***************************************************************/

  /* Enable BKPRAM Clock */

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_BKPSRAM, ENABLE);

  /* Write to Backup SRAM with 32-Bit Data */

  for (i = 0x0; i < 0x1000; i += 4)

  {

    *(__IO uint32_t *) (BKPSRAM_BASE + i) = i;

  }

  /* Check the written Data */

//  for (i = 0x0; i < 0x1000; i += 4)

//  {

//    if ((*(__IO uint32_t *) (BKPSRAM_BASE + i)) != i)

//    {

//      errorindex++;

//    }

  }

whereas i can see the value of sram in memory window

sram even retain the value when i load any other code, just by enabling clock

can you please tell where the issue is? are there any configuration if we connect VBAT that i missed? 

Thank you

 

Posted on March 29, 2013 at 16:44

I don't have any systems with a battery hooked up in this fashion, I typically put the system in standby to turn of the primary supply/regulator.

I think you'd want some different code paths based on whether you're cold starting, or bring a system back from a power event that doesn't require a full RTC initialization.

I might take a look at this, next week, in the context of my own boards, with respect to the (NV)RAM and how it is preserved.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
bl
Associate II
Posted on March 25, 2014 at 09:47

Hin 

Just happened to be reading about this in the Reference Manual RM00090 Doc

did you switch on the Backup domain Reg:-

In 5.1.2 Battery backup domain

''When the backup domain is supplied by VBAT (analog switch connected to VBAT because VDD is not present), the backup SRAM is powered by a dedicated low power regulator. Thisregulator can be ON or OFF depending whether the application needs the backup SRAM function in Standby and VBAT modes or not. The power-down of this regulator is controlled by a dedicated bit, the BRE control bit of the PWR_CSR register (see Section 5.4.3: PWR power control/status register (PWR_CSR)).''

just skimmed you code and couldn't see this being switched on. 

Cheers 

Brian L