cancel
Showing results for 
Search instead for 
Did you mean: 

interfacing between different boards

llwaeva
Associate II
Posted on January 30, 2016 at 06:42

I got a NUCLEO-F446RE, which I use to send control signal to other board via SPI and GPIO. The NUCLEO and the board are powered separately. I wonder do I have to put them to the common ground so to make them work?

2 REPLIES 2
pkumar1883
Associate II
Posted on January 30, 2016 at 06:53

yes you are absolutely right. You will have make Ground common.

Mark Edwards
Associate II
Posted on January 30, 2016 at 19:07

Or use Opto-Isolators if a common 0V would be a problem.