cancel
Showing results for 
Search instead for 
Did you mean: 

Interface 1.8V STM32 to 3.3V SD Card?

frankfrank9
Associate II
Posted on February 18, 2011 at 19:26

Interface 1.8V STM32 to 3.3V SD Card?

4 REPLIES 4
frankfrank9
Associate II
Posted on May 17, 2011 at 14:25

I might add....

Current frontrunner solution is the TI TXB0108.

aqueisser
Senior
Posted on May 17, 2011 at 14:25

We're using the TXS0206 for the same purpose.

Kuikui
Associate III
Posted on May 17, 2011 at 14:25

What you're looking for is a called a ''voltage level translator''.

You just have to be sure it meets your requirements ( In or Out ( or both ), speed, voltage levels, etc ... )

frankfrank9
Associate II
Posted on May 17, 2011 at 14:25

Thanks for the pointer to the TXS family. With its internal pullups it looks like the TXS0108 will be a better fit than the TXB0108.