cancel
Showing results for 
Search instead for 
Did you mean: 

Inquiry on STM32G0 Support for Dual USB-C Ports with DRP and DP-Alt Mode

HungKai.Chien
Associate III

I am currently evaluating the STM32G0 series for a project that requires two USB Type-C ports.
Each port needs to support both Dual Role Port (DRP) functionality and DisplayPort Alternate Mode (DP-Alt).
Can the STM32G0 be implemented?

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @HungKai.Chien 

Indeed, it is the same controller available on both ports. So, they have the same features.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

3 REPLIES 3
FBL
ST Employee

Hi @HungKai.Chien 

Indeed, STM32G0 is the only product using 2 USB type C ports.

You can refer to the MB1352 schematics of STM32G0C1 eval daughter board as a reference.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
HungKai.Chien
Associate III

Hi Support team,


Does each UCPD port on STM32G0C1 support both DRP and DP-Alt mode independently?”

FBL
ST Employee

Hi @HungKai.Chien 

Indeed, it is the same controller available on both ports. So, they have the same features.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL