cancel
Showing results for 
Search instead for 
Did you mean: 

im getting only 0.5v on some gpio pins instead of 3v.

adeemkazi92
Associate II
Posted on October 20, 2015 at 11:29

gpioc pin 0 and gpio a pin 0 &1 work fine

but gpio c pin 1 and furhter show 0.5v at output instead of 3 volts.

here is the code i implemented

&sharpinclude ''main.h''

static __IO uint32_t TimingDelay;

//------------------------------------------------------------------------------

// Function Name : Init _GPIO pins

// Description : pins ,port clock & mode initialization.

//------------------------------------------------------------------------------

void Init_GPIO(void)

{

/* GPIO config */

    GPIO_InitTypeDef GPIO_InitDef;

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);

 

    GPIO_InitDef.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;

    GPIO_InitDef.GPIO_Mode = GPIO_Mode_OUT;

    GPIO_InitDef.GPIO_OType = GPIO_OType_PP;

    GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_NOPULL;

    GPIO_InitDef.GPIO_Speed = GPIO_Speed_50MHz;

    //Initialize pins

    GPIO_Init(GPIOC, &GPIO_InitDef);

 

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

 

    GPIO_InitDef.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;

    GPIO_InitDef.GPIO_Mode = GPIO_Mode_OUT;

    GPIO_InitDef.GPIO_OType = GPIO_OType_PP;

    GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_NOPULL;

    GPIO_InitDef.GPIO_Speed = GPIO_Speed_50MHz;

    //Initialize pins

    GPIO_Init(GPIOA, &GPIO_InitDef);

 

    //volatile int i;}

    }

void Delay(__IO uint32_t nTime)

{

  TimingDelay = nTime;

  while(TimingDelay != 0);

}

/**

  * @brief  Decrements the TimingDelay variable.

  * @param  None

  * @retval None

  */

void TimingDelay_Decrement(void)

{

  if (TimingDelay != 0x00)

  {

    TimingDelay--;

  }

}

/*******************************************************************************

* Function Name : main

* Description : Main program.

*******************************************************************************/

int main(void)

{

Init_GPIO(); //calling a function

while(1)//infinite loop

{

/*ODR bits can be individually set and reset */

//for displaying 0

GPIO_SetBits(GPIOC, GPIO_Pin_0);

GPIO_SetBits(GPIOA, GPIO_Pin_0);

GPIO_SetBits(GPIOC, GPIO_Pin_2);

GPIO_SetBits(GPIOA, GPIO_Pin_1);

}

}

#no-crystal-ball
This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Amel NASRI
ST Employee
Posted on October 20, 2015 at 13:10

Hi kazi.adeem,

I suggest you check the hardware connections to the pins where you see 0.5V instead of 3 V (may be there is an external connection to the ground).

Then, in your main, I don't see the code to set GPIO_Pin_1 for port C.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

adeemkazi92
Associate II
Posted on October 21, 2015 at 07:14

there is no external connection to ground.

and i tried enabling the gpio pins one by one many of them dont set to high

adeemkazi92
Associate II
Posted on October 21, 2015 at 08:26

and these are the pins connected to sb27 to sb 32 these are the jumpers i guess

waclawek.jan
Super User
Posted on October 21, 2015 at 09:42

What hardware are you talking about?

adeemkazi92
Associate II
Posted on October 21, 2015 at 09:44

stm32f072b

waclawek.jan
Super User
Posted on October 21, 2015 at 09:55

I can see no ''sb27 to sb 32'' in the STM32F072 datasheet.

So what hardware are you talking about?

JW
adeemkazi92
Associate II
Posted on October 21, 2015 at 09:59

adeemkazi92
Associate II
Posted on October 21, 2015 at 10:01

here look at the attachment.the pin config is there

________________

Attachments :

Untitled.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0nB&d=%2Fa%2F0X0000000bin%2FKrUVbPrPQt3mDdpO5eDBzWEHcX5XPqTuILxjuYPKssc&asPdf=false
waclawek.jan
Super User
Posted on October 21, 2015 at 10:12

This still does not tell us what hardware are you talking about, nor what is connected to the pins you showed.

Also, you complained about PC1, there is no PC1 shown on that picture.

JW