cancel
Showing results for 
Search instead for 
Did you mean: 

IDE for the STM32F437VIT6?

mrblueblue
Associate II
Posted on July 25, 2016 at 18:15

What would you recommend for an IDE programming for the STM32F437VIT6 with the ST-LINK/V2?

I will be doing some basic things like SPI communcation, I2C, and toggling pins.

Any thoughts on Atollic?  Something else that might be better?

Thanks.

-Mike

3 REPLIES 3
Radosław
Senior II
Posted on July 25, 2016 at 18:22

1. My suggestion is AC6 or the best one clen eclipse distribution with makefile.

2. dev bords check Original ST board (discovery or Nucleo) or much more elastic Waveshare.

AvaTar
Lead
Posted on July 26, 2016 at 08:20

>Any thoughts on Atollic?

 

The downsides, according to my experiences (V5.5.1, free version):

 - limited M7 support (no SamE70 support, but not relevant here)

 - ST-Link support not very robust, and quite sluggish

Debugging an application on a F746 proved rather delicate. Sometimes it didn't find the target at first try, or lost connection. Never had such an issue with IAR, Crossworks, or EmBlocks. Might be related to version V2.1.

And in general, you need to like Eclipse.

mrblueblue
Associate II
Posted on July 28, 2016 at 06:06

Yes, AC6 looks to be an excellent select! Thank you!

-Mike