2025-05-14 1:34 PM
I'm developing LoRaWan project using that uses STM32WL5MOC module and the STM32CubeWL MCU Package (STM32Cube_FW_WL_V1.3.0). I have B-WL5M-SUBG1 module to develop with.
I am seeing that the End Node example does not connect with Chirpstack due to noncompliant DevNonce. It seems I need to patch ST’s CubeWL LoRaWAN End_Node example to make DevNonce persistent across power cycles so that ChirpStack will accept joins).
Has anyone else experienced this? Any insights are welcomed.
Peter
2025-05-14 1:47 PM
Hello @PLaid.1
I suggest you to have a look at this article from Digikey. It gives a description on how to connect the STM32WL to the ChirpStack.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.