cancel
Showing results for 
Search instead for 
Did you mean: 

IAR _ stm32 f4 board => Fatal error: ST-Link, Failed to identify target MCU - Check hardware and interface selected Session aborted!

louati-amir
Associate II
Posted on June 06, 2013 at 19:08

I'm a beginer with IAR.

I selected the st_link for the debugger

but this error is generated :''Fatal error: ST-Link, Failed to identify target MCU - Check hardware and interface selected   Session aborted! ''

I tried one of the project that are included in IAR it work fine. so the problem is not from the driver.
2 REPLIES 2
Posted on June 06, 2013 at 19:19

Do you have SWD mode selected? JTAG mode won't work.

Pay very careful attention to the settings in the project that works, and compare those with the one that fails.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
louati-amir
Associate II
Posted on June 06, 2013 at 19:22

it work now fine think you, it was from that SWD mode :)