IAP: Secure firmware update guidelines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-29 2:17 AM
I've implemented DFU-OTA over GSM network with Fail-back feature (reverting back to older firmware if the upgrade failed, sudden shutdown during the upgrade and in the event of network error) and so far it seem to work fine (Probably I need to test more), However, I would now like to add security features in the upgrade process. I've heard that there could be man in the middle attack, execution of malicious code by reverse engineering the firmware etc. This topic is very new to me, hence I'm looking for guidelines on what and how I should implement secured f/w upgrade.
My firmware binary (My application firmware that will be flashed on the internal main flash memory of STM32F072) will reside on a HTTPS server and I download this binary over GSM network by issuing AT+ command (STM32 MCU is connected to SIM800H GSM module over UART on the custom board). Some of the first few questions that I've in mind are:1: Is it possible to sniff the GSM communication that my board is making, then probably doing a Man in the middle attack won't be very difficult. How to subvert such attempts ?2: Assuming that the HTTPS server where I keep my firmware binary is very robust against attacks (the firmware binary will be uploaded on the server, only after successful authentication), what else can go wrong ?3: Any other guidelines would be also very helpful.Thanks, #iap #stm32f0 #fota- Labels:
-
STM32F0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-04 5:14 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-04 5:37 AM
I don't think you can link the binaries of the ST's crypto library to a PC program. They don't provide the source codes and provide binaries only for different ARM Cortex-M architectures (ARMv6M, ARMv7M) but not for PC (x86/x86_64).
So you'll have to use something different on the PC.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-04 6:49 AM
Hmm, Okay, I've downloaded ARM-GNU Toolchain for windows and trying to compile the code natively (removed printf statements for now). Currently seeing some unresolved symbol issues, but hopefully will resolve it and update here. However, debugging a binary built for ARM on x86 platform is going to be difficult for me. I haven't done anything like this in past before (In past I've used GNU Toolchain to build and flash a different ARM Cortex based MCU but no debugging).
Logs:$ /cygdrive/c/Program\ Files\ \(x86\)/GNU\ Tools\ ARM\ Embedded/5.2\ 2015q4/bin/arm-none-eabi-gcc.exe -o crypto crypto.c M0_CryptoFW_2_0_6.lib -I../../../Libraries/STM32_Cryptographic_Library/inc -I../../../Libraries/STM32_Cryptographic_Library/inc/Common/ -I../../../Libraries/STM32F0xx_StdPeriph_Driver/inc -I ../../../Libraries/CMSIS/Device/ST/STM32F0xx/Include
c:/program files (x86)/gnu tools arm embedded/5.2 2015q4/bin/../lib/gcc/arm-none-eabi/5.2.1/../../../../arm-none-eabi/lib\libc.a(lib_a-exit.o): In function `exit':
exit.c:(.text.exit+0x2c): undefined reference to `_exit'
M0_CryptoFW_2_0_6.lib(crypto.o): In function `Crypto_DeInit':
..\Crypto_Sources_Files\crypto.c:(i.Crypto_DeInit+0x6): undefined reference to `RCC_AHBPeriphClockCmd'
c:/program files (x86)/gnu tools arm embedded/5.2 2015q4/bin/../lib/gcc/arm-none-eabi/5.2.1/../../../../arm-none-eabi/bin/ld.exe: crypto: hidden symbol `RCC_AHBPeriphClockCmd' isn't defined
c:/program files (x86)/gnu tools arm embedded/5.2 2015q4/bin/../lib/gcc/arm-none-eabi/5.2.1/../../../../arm-none-eabi/bin/ld.exe: final link failed: Bad value
collect2.exe: error: ld returned 1 exit status
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-04 6:49 AM
Dear qwer.asdf,
Thank for giving your suggestion.I have included the cryptography pre compiled library file(.a file). So how can linker remove unused section.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-04 6:59 AM
Dear sidekick,
It doesn't seem possible to use ST Cryptography Library(precompiled .a library file) with PC program. Because ST provides these to run on ARM Architecture.(I tried it but didnt work)
So I think it would be better to write a simple code on PC which read a chunk of your raw file and send it to your microcontroller for Encryption. Microcontroller returns back the encrypted chunk.(As suggested by qwer.asdf also)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-04 9:33 AM
Okay. Also, My last post about using GNU Toolchain to build a program linked to ST's crypto library for x86 system was completely useless. For the sake of this topic, It does not matter, what toolchain I use (KEIL's, IAR, GNU etc). How on earth, I'm going to run the cross compiled binary (for ARM target) on x86 platform. Even if i do some emulator (maybe Qemu) to emulate ARM architecture, I would be running the binary on an emulated ARM target platform, __not__ on x86 platform.

- « Previous
-
- 1
- 2
- Next »